Part Number: ONET1191P
I'm confused about the clock frequency vs data rate for the ONET1191p. The datasheet says the part can go up to 11.3 Gbps operation, but the high-frequency 3db BW is as low as 8 GHz (and as high at 15 GHz). And the frequency response data in figure 3 only goes out to ~10.5GHz. Is the 11.3 Gbps data-rate based on dual-edge, so operating with a 5.65 GHz clock signal? Or is it single edge and even though the 3dB point can be as low as 8 GHz, the device can still operate within spec for data-rates with a clock up to 11.3 GHz? If so, shouldn't figures 3, 5 and 6 go out to at least 11.3 GHz? Or am I not thinking about data rate (Gbps) / clock rate (GHz) correctly?
Thanks,