Part Number: DS160PT801
Does the DS160PT801's SMBus interface follow the command formats specified in Intel's "PCIe 4.0 Retimer Supplemental Features" document?
Thanks, John
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS160PT801
Does the DS160PT801's SMBus interface follow the command formats specified in Intel's "PCIe 4.0 Retimer Supplemental Features" document?
Thanks, John
Hi John,
The DS160PT801 has two SMBus modes, 8-bit and 16-bit. When it is in 16-bit mode, it will follow the command formats in the Intel supplemental features document. The retimer is in 16-bit mode on power up by default. You can refer on how to switch between the two modes by using the Programming Guide.
It is important to know that our EVM software, SigCon Architect and Python API, will change the retimer into 8-bit mode when it connects. Most of the Programming Guide is assuming the retimer is in 8-bit mode.
Regards,
Nicholaus
Thanks Nicholaus, but I don't think the device strictly follows Intel's command format. I've eventually been able to access the device in 16-bit mode using standard SMBus register reads and writes. I didn't follow the Intel format where each access starts with a command code byte specifying whether PEC checking is enabled, the function, read or write, and start or end-of-transaction indicators. Can you confirm this?
Thanks, John
Hi John,
I see. Let me look into this and get back to you within 24-hours.
Regards,
Nicholaus
Hi John,
Here is the response.from the design team:
"The short answer is no. We don’t support the command code format in that Intel document.
However, we do support the 16-bit offset address register access described in that document. If the device is in 16-bit mode (the power-up setting) and you access the address according to the Intel document, the corresponding registers inside our device will be updated (on write) or returned (on read)"
So you are correct; It is similar, but not exactly the same. Sorry for the confusion.
Regards,
Nicholaus