Part Number: SN65HVD232
Hi Experts,
Please advise to the query from Cx:
We are using the SN65HVD232D 3.3-V CANBus Transceiver.
Can you tell me what would happen if pin 8 is connected to ground?
I know the datasheet indicates this pin is no-connect, the circuit board designer used the pinout from the SN65HVD251D chip (5V transceiver).
We are troubleshooting an issue where occasionally we are seeing a message we are transmitting essentially get hijacked. Basically we are regularly broadcasting a message with identifier = A and data = B. We are regularly receiving a message with identifier = C and data = D.
Occasionally we are seeing a message broadcast with identifier = C and data = B (in the spot where should see A, B).
During our review we found pin 8 incorrectly handled and wanted to understand what could happen so we can eliminate this as a potential source of the issue.
Thank you.
Regards,
Archie A.