This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I would try a pin reduced approach to sharing a signal for DE/RE# and another for D/R.
Provided that controller will have to change direction of port for D/R signal with proper timing avoiding contention with R, could it be a problem for the transceiver itself?
Thanks
Andrea
Clemens,
thanks for your answer.
From a static point of view I'm sure it will work. I have some concern about the dynamic behavior, i.e. during direction switches. I see in some other posts that somebody experienced unexpected glitches on receiver during TX turnoff.
Provided that shared D/R will be pulled-up, do you expect some erratic behavior during direction switches?
Thanks
Andrea
Assuming that you are using a UART(-like) protocol where the idle state is high, and that you switch directions only when idle, there should be no problem.
Hi Andrea,
Clemens is correct - as long as the enables are being switched during an idle period there shouldn't be much concern (as mode switches could be a bit longer so doing a switching during an idle period - especially in a UART like protocol should be fine.)
Please let me know if you have any other questions!
Best,
Parker Dodson