Other Parts Discussed in Thread: TLV1812, UCC27533, UCC27624
Hi Team,
A customer is looking for a device to simulate an Incremental Encoder. Would you kindly help?
They designed a board with MCU and 2 output signal A and B (image below). These 2 signals are set up with a 90° offset, which is required for the detection of the encoder’s rotation. The characteristics of the 2 signals (A and B): max output current of 20mA, supply voltage from 10Vdc to 30Vdc and short circuit protected

The board is supplied with a voltage from 10Vdc to 30Vdc. There is dc/dc converter and an MCU. The voltage of the A and B signal is the same of the power supply (from 10 to 30 Vdc).
I hope this helps. Please let me know if you need more information
Regards,
Marvin