Part Number: TCAN1043A-Q1
After power up, Is there a way to move this device to sleep mode directly, not going to standby mode which drives INH high.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCAN1043A-Q1
After power up, Is there a way to move this device to sleep mode directly, not going to standby mode which drives INH high.
Kanava,
Unfortunately no, even if both EN and nSTB are in the states that would put the device into sleep mode at power up, it will still first go into standby mode, then immediately transition to sleep mode.
Please let us know if you have any other questions.
Regards,
Eric Hackett
Eric Hackett, Thanks.
Just to be clear, INH will be high after power up (i.e only Vsup > UVsup) even if VCC & VIO are not present (i.e VCC < Uvc & VIO < UVio).
Kanava,
Yes that is correct. And if the EN and nSTB pins are configured for sleep mode after power up, the device should transition to sleep mode from standby mode ~35us after INH is asserted.
Regards,
Eric Hackett
Thanks, I probed INH & Vsup in the EVM board. INH always stayed high, It didn't go low after 35us.
In this setup, only Vsup was connected, no VIO & VCC. Also I added jumper for EN (low) & nSTB (low).
Kavana,
Have you connected any sort of pull-down or load to INH? Note that INH does not pull strongly to GND. It can only either pull high to VSUP or be high-impedance.
When VCC and/or VIO are undervoltage, the device is in sleep mode regardless of the states of the EN and nSTB pins. This makes INH high-impedance. See Table 8-4 for reference.
Best,
Danny
Danny, No I didn't connect any pull-down to INH pin. My observation is not matching with table 8-4. I think after power up (if STB & EN are low) it stays in standby mode.
Hi Kanava,
When TCAN1043A first powers on (Vsup > UVsup), an internal wake request flag is set that will prevent the device from going directly into Sleep mode. To clear this flag, the device needs to be placed into Normal mode (EN = nSTB = high). After this, the device may be place into Sleep mode via go-to-sleep mode (EN = high, nSTB = low). After 20 - 50us in this state, Sleep mode will be entered and the INH signal will move to a high impedance state.
Alternatively, if the transceiver stays in Standby mode for ~4 minutes, the Sleep Wake Error timer (SWE) will time out and the device will automatically move to Sleep mode.
Regards,
Eric Schott