Part Number: SN65HVD1040
Other Parts Discussed in Thread: TCAN1044A-Q1
Hello E2E,
The datasheet said the device has voltage tolerant min -27V to max 40V on CANH and CANL.
Our customer tried test connect 16V DC bias voltage on the communication line (CANH and CANL), that device damaged.
Question;
1. Does the spec have a limit for the voltage superimposed time?
2. Is the purpose of the spec to allow transient voltages on the communication line, and is it not supposed to be short-circuited with other circuits?
Best regards,
ACGUY