Part Number: TL28L92
We are facing an issue while transmitting data. As per data sheet, when the external clock is used by the transmitter in pin IP3, the transmitted data is clocked on the falling edge of the clock. But our transmit data when probed on an oscilloscope shows the converse. Please see the attached scope image.

Also, we don't find a method in the datasheet to reverse the edge polarity. Why does this happen?
The DUART chip configuration is given below:
Normal mode
16 byte FIFO
interrupt when one or more bytes are received
disable watchdog
RxRTS control on
RxRDY interrupt enabled
block error mode
no parity
8 bits/char
normal channel mode
no TxRTS control
CTS enable of transmit
1 stop bit
receive clock = IP4 (1x)
transmit clock = IP3 (1x)
The DUART pin level details are attached.