This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LVDS822: Availability of SN65LVDS822EVM? Provide GERBER files?

Part Number: SN65LVDS822
Other Parts Discussed in Thread: SN65LVDS93B

Team,

I cannot find the SN65LVDS822RGZEVM board listed on TI.COM.
-Has it been discontinued?
-Could we make the GERBER file available so that customer could build it and use samples to make some tests?
-What would be the closest EVM still available/orderable from TI.COM?

Thanks in advance!

A.

  • Hello A.,

    1. Yes, this board is no longer manufactured.
    2. You may refer to SN65LVDS822 User’s Guide (Rev. A), which has the EVM schematics and a picture of the EVM layout. 
    3. This is an older device so similar EVMs are harder to come by. Could you provide more information on your system needs? What kind of interfaces are being used? Do you require compatibility with a specific device? What is the general topology?

    Best Regards,

    Melissa

  • Hi Melissa,

    Yes we (Customer and I) saw the EVM UG - SLLU184 with the different info inside.
    But in this case we need the source file of the GERBER.

    Customer would need to do some validation test of SN65LVDS93B based designs and need some HW to do so.
    Using the GERBER they would re-do a PCB in order to test this system.

    -Can you please double check if you can find the SN65LVDS822RGZEVM GERBER file?
    -Alternatively can you provide an EVM board or Gerber file of an other TI devices that could be used to test a design using SN65LVDS93B?

    Thanks in advance,

    A.

  • Hello A.,

    Please check your email for the Gerber files.

    Best Regards,

    Melissa