Part Number: DP83867IR
Hello
Our customer is investigating to employ DP83867 for new project.
There is tight PCB space limitation, they want to minimize number of external resistors for pin strap under SW control mode.
Which pin strap is mandatory to place resisters to keep basic function?
On the datasheet, it seems following function can be initialized by SW registers setting. Can we reduce pin strap for those pins?
RX_D5 pin: Force MIDI/X, Half-Duplex Enable
RX_D6 pin: AMDIX Disable
RX_DIV/RX_CTRL pin: Auto Disable
CRS pin: Fast Link Drop
LED_0 pin: Mirror Enable
Regards,
Mochizuki