This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IR: Mandatory pin straps

Part Number: DP83867IR

Hello

Our customer is investigating to employ DP83867 for new project.

There is tight PCB space limitation, they want to minimize number of external resistors for pin strap under SW control mode.

Which pin strap is mandatory to place resisters to keep basic function?

On the datasheet, it seems following function can be initialized by SW registers setting. Can we reduce pin strap for those pins?

 

RX_D5 pin: Force MIDI/X, Half-Duplex Enable       

RX_D6 pin: AMDIX Disable

RX_DIV/RX_CTRL pin: Auto Disable

CRS pin: Fast Link Drop

LED_0 pin: Mirror Enable

 

Regards,

Mochizuki