Part Number: DS90UB954-Q1
Hi Teams,
I2C is used for register setting and back-channel of the 954.
The SoC connected to the 954 has the SSCG setting enabled for the internal PLL.
Therefore, it appears that the I2C clock is also SSCG enabled.
Is it OK to input SSCG to the I2C block of the 954?
The SSCG settings to be input are as follows.
1.Down spread
2.Modulation 3%.
3.Modulation frequency 4.03kHz
What is the allowable range of SSCG, if any?
Best Regards,
Masanori