Part Number: TCA9517
Other Parts Discussed in Thread: TXU0304, SN74AXC4T774
Hi TI Team,
Please help to check the schematic diagram of TCA9717 is it feasible?


B/R
Adan Wu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Adam,
To further add on to Clemens response, it is suggested to populate R61~R63 for the I2C signals in order to propagate a signal high. It is also recommended to use 0.1uF for the values of the bypass capacitors (C72 and C73). However if the value you are currently using mitigates the visible noise, then it is OK as well.
Regards,
Jack