Part Number: TLIN1024A-Q1
The proper connection of Vsup1/2 is confusing as the datasheet shows multiple ways to do that. The connections for the pullups for commander mode are also not clear.
- Figure 9-1 and Figure 12-1 show that Vsup1 and Vsup2 both need a connection to Vbatt through a diode and cap
- Figure 10-1 shows Vsup2 not connected to Vbatt and the pullups on LIN3 and 4 are pulled up to Vsup1.
What is the proper way to connect Vsup1, Vsup2 and where should the pullups/diode be connected to for each of the 4 channels in Commander mode ?