Part Number: DS90UB928Q-Q1
Other Parts Discussed in Thread: ALP
What’s the recommended way to control OEN & OSS_SEL, when I want to enable GPIO and LVDS pins of the DS90UB928?
DS90UB928 datasheet states on chapter 9.4:
“OEN should be enabled LVDS outputs after PDB turns to high state and the internal circuit is stabled.”
Should I connect the OEN & OSS_SEL pins like this, if I want to enable outputs permanently?

Isn’t it possible to activate the UB928 outputs by writing the registers?
I left the OEN and OSS_SEL pins of the DS90UB928 floating. Then I set the OEN and OSS_SEL bits in the “General Configuration 0” register, but the outputs are not activated. This register writing doesn’t seem to do anything, although both registers are RW. I’m using the ALP software for the (remote) register writing. Am I missing something here?