Other Parts Discussed in Thread: TFP401
Please help with the following:
On the datasheet it shows the max power on page 6 as being 370 mA, I am running this in a 1 pixel/clk mode instead of 2pixel/clk mode and using even outputs not the odd outputs.
Question: what is the typical power number for this part in this case?
ODCLK is 165Mhz and 1 pixel per clock, and only the even outputs.
Question: Does this make a difference in the current draw Idd, and what is the typical current draw?
Thanks