This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9803: Connecting TCA9803 B side to I2C Mux (Pass-Gate based)

Part Number: TCA9803
Other Parts Discussed in Thread: PCA9548A, TCA9509

The DS states not to connect B PU on the B-Side because of the internal current source. 

I would like to know if the below connection is problematic (having I2C MUX PCA9548ABS) after the TCA9803

  • The PCA9548A is a pass-gate mux; the pull-up resistors of the enabled channels are connected to the TCA9803's B side.
    This is not allowed.

    Exchange the A and B sides, or use a different translator like the TCA9509.

  • Hey Dror,

    As Clemens' mentioned, this will be an issue when the PCA9548A drives a low- the internal FET closes (rdson becomes low) and then current flowing from the 4.7k PU will be seen at the TCA9803, which violates IEXT-I. 

    Regards,

    Jack