Part Number: SN65DSI86EVM
Other Parts Discussed in Thread: SN65DSI86
Hello,,
CPU ; I.MX8MQ MIPI(DSI)
LCD ; AUO G133HAN02.0 (2 Lane eDP 1.2)
Connect to LCD using MIPI(DSI) eDP Bridge.
Is it possible with sn65dsi86?
Thanks in advance.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65DSI86EVM
Other Parts Discussed in Thread: SN65DSI86
Hello,,
CPU ; I.MX8MQ MIPI(DSI)
LCD ; AUO G133HAN02.0 (2 Lane eDP 1.2)
Connect to LCD using MIPI(DSI) eDP Bridge.
Is it possible with sn65dsi86?
Thanks in advance.
Hello,
Is this the datasheet you are referring to: www.displaytechnology.co.uk/.../g133han02.0_datasheet.pdf
Under review it supports the
- All input signals are eDP (Embedded DisplayPort) interface compatible -> SUPPORTED
- 2 Lane eDP 1.2 -> DSI86 is COMPATIBLE with eDP 1.4 and backward compatible with 1.2
- FHD 1920x1080 /60Hz-> SUPPORTED
- CLK freq = 70.5 MHz typ. -> SUPPORTED
Thanks,
Zach