Part Number: DS90UB960-Q1
Other Parts Discussed in Thread: DS90UB953-Q1
We design and build camera with SER-DES architecture.
The SER is UB953, and the DES is the UB960.
The SER + cable side works well (tested on DES EV boards).
Registers 4d and 4e indicate unstable link.
Attached the values of these registers, that were read at 1 second intervals.
R: 0x4D 0x4E --------- 0x37 0xe9 0x33 0x28 0x33 0x28 0x30 0x2c 0x33 0xed 0x30 0xe9 0x30 0x28 0x33 0x28 0x37 0x28 0x30 0x28 0x30 0xeb 0x33 0x28 0x33 0xe8 0x33 0x28 0x37 0xe8 0x33 0x28 0x33 0x28 0x37 0x2c 0x33 0x28 0x33 0x69 0x37 0x28 0x37 0x28 0x37 0x69 0x30 0x28
Is it possible to infer anything related to the cause of the problem from this data?
Are there others ub960 registers that could help us to diagnose the unstable link?
Thanks