Part Number: TCAN1044A-Q1
Other Parts Discussed in Thread: TCAN1044-Q1
> The V devices have an I/O voltage level translator.
If the description above is correct, which makes sense, then there is a typo in the TCAN1044-Q1, TCAN1044V-Q1 datasheet SLLSF17B – AUGUST 2019 – REVISED OCTOBER 2021
The datasheet (at 1st page, section 3 Description) and Product details on https://www.ti.com/product/TCAN1044-Q1?keyMatch=TCAN1044#description web site says
"The TCAN1044-Q1 includes internal logic level translation via the VIO terminal to allow for interfacing the transceiver I/Os directly to 1.8 V, 2.5 V, 3.3 V, or 5 V logic I/Os."
Is there a missing V in device part number? Can you double check and confirm.
We are make list of device alternative part numbers and I want to be sure that we have correct devices on the list. Thank you.