Part Number: DP83849I
Hello team,
I received a question from the customer.
Is the only way to stop the output of the SLP signal, etc., by controlling the RESET signal?
The customer's situation is as follows,
During normal use, the device is operated with PWRDOWN_INT = High, but the register setting value is to be used as it is, so the customer wanted to control PWRDOWN_INT = Low instead of RESET control, so that no waveforms are output to the Ethernet pin. However, when the auto-negotiation function is turned off, even if PWRDOWN_INT = Low, the SLP signal is output and the link up/down is repeated. So, is the only way to prevent the SLP signal from being output, etc., by controlling the RESET signal?
Regards,
Masa