Part Number: DP83867CR
Hi,
I have dual PHY ic connected to zynq processor. Both sections are same in both hardware and software aspect. I am able to ping only one PHY but not the second PHY
Both links are up. But second PHY speed is limited to 100Mbps. (PHY 2 is being detected by processor by reading 0xa231 in reg 3)
1. I have tried with same ethernet cable and same link partner as that of PHY 1.
2. I have given software reset by writing to 0x1000 to 0x001f
3. I have tried by disabling 10mbps and 100Mbps to force 1Gbps speed (this was there in some answer in the forum).
4. I have tried by writing 1 to 9th bit of 0x0009 reg(. Configuration Register 1)
Please help
Regadrs,
SCH