Part Number: DS90UB954-Q1
Other Parts Discussed in Thread: DS90UB935-Q1, DS90UB953-Q1, USB2ANY
Hi,
We are using DS90UB954-Q1 this serializer in our board, it's interfaced on the i2c. On the same i2c two devices are connected one is responding properly but DS90UB954-Q1 device is not responding. its showing error as Remote I/O error. i am following sequence for the reading the register of the serializer. wrting device addres , register address , then reading the by providing the device address. when i am sending device address only its giving an error. i confirmed the device address its correct by referring the datasheet .

We are trying local i2c read and write. We are using 7 bit address only because that function will covert to 8 bit add the wr/rd bit inside this function. Power down pin at the high state only after the power sequence.