Part Number: TLIN1029-Q1
Other Parts Discussed in Thread: TLIN1027-Q1, TLIN1029A-Q1
Hi Guys
I have a customer that does a very low Baud rates and they see the reset on the Low bauds as the Chip thinks it’s an error on the bus.
Is there a way to override the TXD Dominant time out protection (DTO) state or would they have to go with TLIN1027 device without the DTO function incorporated?
The problem is the 5 baud init sequence which has a wait time of 200ms between bits. It detects anything over say 80ms as an error.
They hoping that there is a know work around to disable the state on the 1029 chip.
Thanks
Rodney