Part Number: SN65DSI86EVM
Other Parts Discussed in Thread: SN65DSI86, DSI-TUNER, SN65DSI84-Q1
Hello everybody,
i have a question about the SN65DSI86, in particular the SN65DSI86-EVM.
We are using a display with the PS8625 DisplayPort to LVDS converter and need to adapt the display to a MIPI-DSI-MCU from NXP. The display is working fine if i connect it directly to a computer running either linux or windows.I am using the SN65DSI86-EVM and want to test out the testpattern first before we connect it to the MCU-Eval-Board and start writing code. But i am not able to get it to work.
The edid data programmed in the display I2C-EEPROM looks like that:

I got the edid file from the display-supplier and opened it with a edid editor.
My settings for the DSI-Tuner are the following:
We have only two DisplayPort datalines and the AUX-lines i tried different combinations of polarity and even bits per pixel although it should be 18 (6bits per color). I am not sure about the SSC-Part i also tried enabling and disabling but nothing worked. It is not connected with the MCU-Board and the MIPI-Lines are just unconnected therefore i want to try the testpattern. For that i set the 0x3C Register to 0x10. The backlight is controlled by the LVDS-Converter on the display, so no need in the first place. My setup is the display that uses a special connector therefore i adapt it via a custom pcb to change it to Displayport and Power-In. On that board i can set the HotPlug-Pin to 3V3 or GND, which works fine with a computer.
After plugging everything in and supplying the Display with power i turn on the EVM, reset it, search for the converter via a i2c sniffer and write the configuration to the chip but nothing works. Here are my generated settings. The clock is generated by the crystal on the EVM.
Any ideas?
Thank you very much in advance.
0x09 0x00
0x0A 0x03
0x0D 0x00
0x10 0x3e
0x11 0x00
0x12 0x4c
0x13 0x4c
0x20 0x20
0x21 0x03
0x22 0x00
0x23 0x00
0x24 0xe0
0x25 0x01
0x2C 0x06
0x2D 0x00
0x30 0x03
0x31 0x80
0x34 0x2e
0x36 0x17
0x38 0xd2
0x3A 0x16
0x3C 0x10
0x3D 0x00
0x3E 0x00
0x5B 0x01
0x93 0x25
0x94 0x20
Here is the info from the display datasheet: