This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75DP139: Do we have device to support the device support HDMI to DVP?

Part Number: SN75DP139


Hi team,

      Our customers want a bridge to support HDMI to DVP. The more details are shown below. I could not find a device to meet the customer need. Could you please recommend a device?

信号传输方向[Signal Transmission Direction] HDMI to parallel port
协议版本[Protocol Version] HDMI1.4 (need to be certified)
其他特性[Other Features] The signal type supports HDMI 1.4 input and parallel DVP output;
Support RGB444 and YUV422 output in video format;
Support audio input and output; can meet HDMI1.4b sink certification;
The ambient temperature supports -20°C~85°C.
最低工作温度[Ta(Min.)] -20℃
最高工作温度[Ta(Max.)] 85℃

 

YOURS

NAN