Part Number: TCA9546A
Hi TI team,
We want to use TCA9546A on our design, but we have concern for datasheet.
Please refer our diagram.


VCC=3.3V and Vpass is about 1.9V .
About Vpass min is 1.6V on VCC 3V to 3.6V.
In order for the TCA9546A to act as a voltage translator, the Vpass voltage must be equal to or lower than the lowest bus voltage.
If our design in VCC=3.3V case, our master use 1.8V but Vpass is in 1.6V-2.8V.
We're worried about this in 1.8V master side.
Do you have experience and suggestion for this design? Do we have any risk? or we must change to VCC in 1.8V.


BR,
Helen