Part Number: PCA9306
All, a large customer would like to enable 16 PCA9306 with the same GPIO.
Using figure 9.2 as the base, Vref=1.2V and Vref2=3.3V, GPIO is 3.3V.
Is it as simple as connecting all EN together? how much drive current is needed from the GPIO, does the 200K resistor need to be changed, do I need 16 resistors?
Thanks,
Regards,
Joe