Other Parts Discussed in Thread: TPL9202
Hello,
I am planning to use two TPL9202's to drive HE751A1200 relays from Hamlin and EV-2M-12 Solenoid Valves from Clippard. I am interfacing the TPL9202 to 5V SPI bus that have individual Chip Selects. I have connected the OUTn pins to the respective Relays and Solenoids. Do I need to use any protection diodes on the output ?
The Relays would consume about 0.15 W and the Solenoids would consume about 0.67 W. I have connected the Exposed PAD to GND plane on my PCB.
A Snapshot of the schematic is as below. I would request you to kindly review the same.

Thanks and Regards,
Naveen