Part Number: PCA9555
Dear TI member,
We know the INT pin is cleared by BIOS read IO expander.
We want to confirm that if the interrupt occurs after entering the OS, how can the IO expander INT pin be cleared?
Thanks.
Ariel
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PCA9555
Dear TI member,
We know the INT pin is cleared by BIOS read IO expander.
We want to confirm that if the interrupt occurs after entering the OS, how can the IO expander INT pin be cleared?
Thanks.
Ariel
The interrupt is cleared when the port register has been read (see section 8.4.1 of the datasheet). Any edge on one of the port's inputs that happens afterwards will re-enable the interrupt.
If that happens, it is usually not a problem; the interrupt handler will simply be called again.
Hi Clemens,
Thanks for reply.
We want to confirm the behavior of io expander when entering the OS.
Under the OS, the bios has delivered control to the OS.
If we need to clear the INT pin at this time, how can we achieve it?
Thanks.
Ariel
To clear the interrupt, read port input register.
I do not know what BIOS or OS you are using, or what their responsibilities are.
Ariel,
I agree with Clemens' answer.
Conduct an I2C read on the input port register to clear the interrupt flag.
I am unsure about your point on the OS/bios. Can you provide a little more context to your situation?
Regards,
Tyler