This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TVP5150AM1: Analog Video Delay Line ICs

Guru 15050 points

Part Number: TVP5150AM1

Hi,

With the EOL of the ISL59920, I am looking to see if TI has an equivalent product.
As far as I can see on the web, there seems to be no applicable TI product, but let me check just in case.

Renesas: ISL59920
https://www.renesas.com/jp/ja/document/dst/isl59920-isl59921-isl59922-isl59923-datasheet?r=501791

The required specs are shown below.
・-3dB BW: 153MHz or more
・Adjustable Delay: 60ns or more
・The control method does not matter.

Thanks,

Eevee