Part Number: DS90UB964-Q1
Hi
The customer has a problem, as shown in the picture below, there are four camera in channels on the left, and two CSI out channels in the green circle on the right May I ask how to use these two CSI outs? Based on the total input data rate of the left camera, decide whether to use one CSI output or two CSI outputs on the right side? If yes, is it necessary for the SOC to have two independent PORT CSIs with virtual channels to take out four CAMERA screens? If not, how to use these two CSI out?