Part Number: DP83822I
Hello,
does the internal Packet Generator (BISCR = 0x0016 Bit 12) need an external CLK (25 MHz) on Pin X1 to generate vaild Data? Or can I perform an BIST without an present CLK-Signal on Pin X1?
Thanks for helping.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83822I
Hello,
does the internal Packet Generator (BISCR = 0x0016 Bit 12) need an external CLK (25 MHz) on Pin X1 to generate vaild Data? Or can I perform an BIST without an present CLK-Signal on Pin X1?
Thanks for helping.
Hello Kevin,
A clock on XI or a crystal between XI, XO is needed.
--
Regards,
Gokul.