Part Number: TCA9803
Other Parts Discussed in Thread: TCA9800, TCA9517, TCA9509
Our new product has the following I2C configuration:
- One I2C bus master board and 5 slave boards, all on the same bus
- Boards are connected by short cables
- All boards run at 3.3V
We want to put TCA9803 devices on the master and slave boards in the following configuration. Our use case is buffering only, without level-shifting. Can you please confirm that this setup is correct? Thank you!


We want to thank the TI team for offering (by far) the best I2C product line! We always turn to TI for all our I2C device needs.