Part Number: TS3USB30E
Hey,
We are using this switch with I2C signal to connect it to two different cameras.
The input I2C signal is pulled up to 3.3V while the cameras need 1.8V.
I was wondering if the input and outputs are buffered and so allow to connect the outputs with PU to 1.8V like in the pic below or is a level shifter needed?

thanks,