This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90LT012AQ-Q1: level shift 3.3V to 1.8V / IBIS-Model

Genius 17485 points

Part Number: DS90LT012AQ-Q1
Other Parts Discussed in Thread: DS90LV012A, SN65LVDS4, SN74AUC1G125, SN74AXC1T45-Q1

Hi all

My customer is running simulations for the DS90LT012AQMFE/NOPB  using the IBIS-Model from the TI page:

https://www.ti.com/lit/zip/snlm044

In the IBIS-Model Pin 8 is the TTL_Out but in the datasheet and in their design it is Pin 5.

Do they use here the wrong IBIS-Model? If yes, is there another model available ?

-------------------

Moreover they want to level shift the output from 3.3V to 1.8V, what device can you recommend to do that ?

Best regards

Ueli