Part Number: DP83TC812S-Q1
Hi there,
The PHY has been connected to one of the port on a managed switch. The path looks like,
managed switch -> PHY -> T1-TX MediaCovnerter -> RJ45 -> Linux machine
The MC used in this case is EVB-LAN8770M_MC.
The PHY has been configured as slave per SNLA389A and the switch port link show active along with the MC Link LED Green.
However,
- When trying to ping the Linux machine from the switch VLAN, the port is only able to Tx transmit the packets and DOESN'T Rx receive any packets.
- From the other side as well the observation is same, if trying to ping VLAN from Linux machine, the machine only Tx transmits packets but DOESN'T Rx receive packets.
- ABLE to ping switch VLAN via other CuPHY interface from the Linux machine
Does PHY registers needs to be configured to be able to receive packets?
How do I troubleshoot this? Is there any guide already?
Gerome Cacho Appreciate any help.
thx,