This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83826E: DP83826E RX_CLK/TX_CLK idle in MII mode after PHY reset

Part Number: DP83826E


The PHY has a 50Mhz input clock on the XI pin that is stable.  I have backported the TI driver from 5.15 linux to 4.1 linux.  All x_mmd routines that access the PHY registers were replaced with routines that use the MDIO bus to communicate.  All read/write testing of registers successful and values are good.

When stopping in U-boot, the PHY is soft reset through the BMCR register.  The PHY will successfully auto negotiate,  and the ETH interface works fine.

Probing of the RX_CLK and TX_CLK pins shows a valid clock.

When the system boots, the MAC driver discovers the PHY and calls the driver reset function.

The TI driver uses the PHYRCR (0x1f) register to do a hard reset, and validates that the reset bit clears.

Afterwards, the RX_CLK and TX_CLK are idle.  The PHY RX_CLK/TX_CLK signales are connected to a CYCLONE5 FPGA that needs these clocks active for its own reset functionality,  

This initialization fails, and the ETH interface cannot be brought up.

I tried writing 0x0200 to BMCR to start auto negotiation but this has no effect on enabling the clocks.

What am I missing in the setup to get the RX_CLK/TX_CLK signals running again after the reset?

  • Hello Kerry,

    You mention that the clock on XI is 50MHz which indicates the PHY is planned to be configured as RMII Slave. In RMII Slave, we expect no clock output on RX_CLK and TX_CLK pins.

    When you say that you see valid clock on RX_CLK and TX_CLK, what is the frequency of the clock?

    --
    Regards,
    Gokul.