Part Number: DS90UB948-Q1
Dear expert,
Can one UB941- one UB948 connect with two screen? UB948 has two OLDI interface. Can it support 2x single OLDI mode to support two 1280*720 screen?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB948-Q1
Dear expert,
Can one UB941- one UB948 connect with two screen? UB948 has two OLDI interface. Can it support 2x single OLDI mode to support two 1280*720 screen?
Thanks
Hi Ryan,
Yes, you should be able to use the UB948 with the UB941 to output to two different screens.
Section 7.4.1 of the UB948 Datasheet has more details regarding this, and there are also some E2E threads detailing how these videos need to be sent from the SOC and processed.
Please let me know if you have any other questions or concerns.
Thanks,
Ryan