Part Number: MAX3243
Other Parts Discussed in Thread: SN74LVC1G07
Hello team,
On the datasheet, it's difined that the V_OL is max 0.4V when I_OH=1.6mA.

What is the maximum output for the I_OH? Can it go up to 3 - 5mA?
If that's possible to achieve I_OH=3 - 5mA, then waht would be the V_OL at that condition?
Best Regards,
Kei Kuwahara