Part Number: SN65LVDS050
There wasn't any information on the datasheet with regards to unused I/Os for the driver AND receiver.
Do I need to tie them to VCC or GND directly or through a resistor? Or do I need to leave them hanging?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65LVDS050
There wasn't any information on the datasheet with regards to unused I/Os for the driver AND receiver.
Do I need to tie them to VCC or GND directly or through a resistor? Or do I need to leave them hanging?
Hello AH,
You can leave these pins floating. Just note the output of the receiver will give a Logic High, while the driver gives a Logic Low for output Y and Logic High for output Z.
Regards,
Josh
No; shorting outputs to the wrong voltage would greatly increase the power usage. Unused outputs should be left open. (In general, inputs should not be left floating, but this device has internal pull-up/-down resistors at all inputs.)
A differential output always has one of its pins in the high state. Such a DC voltage on an unconnected pin is not a problem.