Part Number: TUSB422
Hi Team,
1: We don't have an evm board. Does this macro control have to be enabled?
CONFIG_ TUSB422_ PAL=y
2: We enable CONFIG_ TUSB422_ PAL and compile error occurs. Do I need to modify the contents of these files or can you provide them? If you could help, our kernel is version 5.4.
#include <huawei_ platform/usb/hw_ pd_ dev.h>
3: In the tusb422-pd.txt dts configuration file, if there is an evm board, there is a configuration mode. If there is no evm board, could you tell us how to configure the power supply VCC3.3V and VCONN5V and how to configure the power supply VCC in the dts? For example, the connected VCC is VDDIO_ D_ 2. I'd appreciate it if you could give me references.
4: I refer to the driver tusb422-pd.txt document, and the interrupt configuration is ti, alert-gpio=<&gpio1 16 GPIO_ ACTIVE_ HIGH>;, What does gpio1 mean and what does the middle 16 mean? The main control terminal GPIOH _ 4. Could you tell me how to configure it?
Kind regards,
Katherine