Part Number: DP83848I
Hi,
I am interfacing DP83848IVV with STM32F765ZGT6. This design is a new version of old design. In old design I was able to successfully interface the PHY with STM32. But in new design same code is not working. There has been no change in the Ethernet circuit. On CRO, I see that RCC_MCO is 25MHz, and CLK_OUT is also 25MHz. I do not see any 2.5MHz clock on MCO - which means that communication is not working.
Physically circuit is okay and I checked on 3 boards. On all new boards the ethernet is not working. In old board the ETH_RXDx and ETH_TXDx lines were around 96mil. In new board these lines are 106mils. Operating in MII mode.
Please suggest what should be correct way to debug and identify the issues.