Part Number: MAX232E
Hi
I am using an MAX232E in a motor control application. between controller and motor.
The block diagram of the product is shown below.

Some users are having trouble with MAX232E failure.
Both the motor side and the controller side will fail. The probability of occurrence is higher on the controller side.
Failure mode does not output TX.RX is normal.
CH1:14pin(DOUT1) CH2:DIN1

After investigating the fault, I found that the Vs-(6pin) was not functioning properly.
case1:not work

case2:positive voltage

case3:Voltage instability at output

The cause of the failure that I presume is the following, but the failure cannot be reproduced.
1.The GND line is disconnected and the power supply voltage is being applied to the IC.
2.Failure due to surge noise from motor.
3.Damage from ESD
Also, when a failure analysis was performed by a third-party organization, internal destruction of pins 14(D1out) and 15(GND) was confirmed.

Vs-(6Pin) is broken in short mode.
If anyone knows the cause or has experienced similar symptoms, please let me know.I will provide any information you need.