Part Number: DP83867CS
Other Parts Discussed in Thread: DP83869HM, , DP83867E
HELLO
Please tell me about the phase noise mask specification for the Clock In (XI) pin.
【Question1】
Please tell me about the following 25-MHz Oscillator Specifications.
The following phase noise mask specifications are in the DP83867CS but not in the DP83869HM.
Why is it only in the DP83867CS?
【Question2】
I have selected a crystal oscillator, but I cannot find a part that meets the following specifications.
Are the following specifications always required?
Also, what kind of impact will occur if the following requirements cannot be met?
◇25-MHz Oscillator Phase Noise
・10Hz :-90[dBc/Hz](MAX)
・100Hz :-90[dBc/Hz](MAX)
・1KHz :-100[dBc/Hz](MAX)
・10kHz :-125[dBc/Hz](MAX)
・100kHz :-125[dBc/Hz](MAX)
・1MHz :-125[dBc/Hz](MAX)