Part Number: AM26C32
Hello Experts,
We have a question about AM26C32 fail safe feature.
Cx configuration is shown below:
There are two data channels that fed two AM26C32 inputs. One of this channel is driven while the other is in high impedance state. At the same time, one line receiver is enabled while the other is enabled (this should not interfere with the input fail safe).
[1] What is reliable the fail-safe when two inputs are connected together like the attached circuit?
[2] Could the input impedance (of the circuit reported at page 8 of the AMC32 datasheet) load the fail safe network of the enabled line receiver while the bus is in high impedance state and perturb the output high state?
Thank you for your support.