Hi Team,
My customers are facing a problem when using TCAN1145. Currently they are communicating with a positive common voltage on CAN bus. When they short the CANH and CANL to GND, TCAN1145 is not entering the fail safe mode, but it is still communicating with 0V common mode voltage on CAN bus.
However, it should be considered as a fault from customer's view since it is already shorted. And because there is no diagnostic function of TCAN1145, it cannot be read by SPI as well when there is no fail safe mode.
Why are the TCAN1145 not entering fail safe mode when CANH and CANL are short to GND? Could the big common mode choke be a reason?
If the TCAN1145 consider the above scenario is not a fault, how could it be detected via SPI?
Your support will help us a lot, thanks !
Manu