Part Number: TCA5013
Other Parts Discussed in Thread: TIDA-00382
Hi
TDA5013 Having 3 SAM slots and 1 User card slot, If i use SAM card in the user slot, will it work compatible like SAM slots?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCA5013
Other Parts Discussed in Thread: TIDA-00382
Hi
TDA5013 Having 3 SAM slots and 1 User card slot, If i use SAM card in the user slot, will it work compatible like SAM slots?
yes, you can use sam card in user card slot.
Regards
Brian
Thanks Brian,
But need more Clarification..
1. IOMC1 & CLKIN1 and IOMC2 & CLKIN2 of TCA5013, is this pins are compatible to connect Host(Mc) ISO7816 UART pins.
2. Clarification needed, how we can interface the SAM card in the user card place? PRES, C4, C8 PINS can be left floating or we should pull down or pull up.?
3. TIDA-00382 EVM board -- How can we procure or rented for particular period for better understanding in TCA5013?
4. Any reference design or file available for TCA5013 with 4 SAM interfaced?
1; should compatible to ISO7816-3 UART pins
2: PRES need to pulldown , C4/C8 is open drain , so just floating
3:you may can get schematic
4: I do't see a design with 44 SAM card yet.
we will help reviewing schematic, but don't support software.
regards
brian