Part Number: TLK1501
Hi,team,
My customer has the following questions,
"I would like to know the cable length limit (guideline) when using the TLK1501 (0.6-1.5Gbps transceiver) with copper cable. Two patterns when the serial data speed is set to 0.6 Gbps and 1.25 Gbps as conditions.
In addition to the cable length limitation mentioned earlier, is it possible to convert the TLK1501 serial signal CML → LVDS and isolate it with a high-speed LVDS isolator? Generally, I think that 1.25Gbps optical transceivers are used, but we are considering whether it is possible to use different physical layers according to the distance and required band, so if you have any examples, could you please give us information? Thank you for your cooperation."
This is very important for my customer, please give some suggestions, thank you.
Regards,
Katherine