This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB948-Q1: Display and camera interfacing options and information

Part Number: DS90UB948-Q1
Other Parts Discussed in Thread: SN65LVDS93B

Hello Team!

Related to the previous question, I would also like to know whether there is a way to interface between MIPI CSI and MIPI DSI, as in some component that can do the interfacing between these two formats and/or a document that explains how this can be done from the software side with alternative solutions.

I was also unable to find any information in regards to DPI and e/DP formats, is there a series of serialiser/deserializer ICs that can handle interfacing with these as inputs and delivering the output on a far display where it is preferably deserialized into DSI or OLDI?

Thank you in advance,

Nuri 

  • Hi Nuri,

    I would like to clarify what exactly you're looking for.

    1.) Are you looking for a setup that can take a MIPI CSI Input and have a MIPI DSI output or vice versa? Or are you looking for a system that can input CSI and/or DSI with a different output?

    2.) You are asking if we have DPI or e/DP to DSI/OLDI correct? We do support this setup, the DS90Ux983 is capable of taking e/DP inputs and can work with FPD3 or 4 deserializers to output to oLDI. We also have the SN65LVDS93B which should fit the need for DPI to oLDI.

    Thanks,

    Ryan

  • Hello Ryan,

    1) Yes, I am looking for a setup that can take a MIPI CSI Input and have a MIPI DSI Output.

    2) Yes, that answers my question perfectly!

    Thank you for your support!

    Nuri

  • Hi Nuri,

    Unfortunately, we do not have any setups which support a CSI input to a DSI Output at this time.

    Thanks,

    Ryan